cancel
Showing results for 
Search instead for 
Did you mean: 

any different of EOLed ST72F561J9TBXS vs ST72F561J9TAS? any replacement MPN?

Vivi
Associate

Temperature range A = -40 °C to 85 °C and C = -40 °C to 125 °C

but ST72F561J9TBXS Datasheet not mentioned suffix B temperature range, could you please share? thanks!

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Peter BENSCH
ST Employee

Welcome, @Vivian Wang​, to the community!

these particular microcontrollers were discontinued a long time ago, but were also not generally available, as they were custom devices that only the specific customer had documentation on.

There are also no substitutes for these devices.

If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Vivi
Associate

Hi Peter, regarding ST72F561J9TAS suffix A means Temperature range A = -40 °C to 85 °C and C = -40 °C to 125 °C how about ST72F561J9TBXS ? Datasheet not mentioned suffix B temperature range, could you please share? thanks!

When a device is obsolete, I no longer have any support or documentation at all.

Sorry for not being able to help you in this case.

Regards,

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thought TB was -40 to 125C, TA was -40 to 85C

The other more standard suffix method, ie

ST72F561AR9T6

Where 6 = -40 to 85C, 7 = -40 to 105C and 3 = -40 to 125C

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..