cancel
Showing results for 
Search instead for 
Did you mean: 

[ANN] eLua (Lua for microcontrollers) 0.4 released

darkore
Associate II
Posted on September 02, 2008 at 17:20

[ANN] eLua (Lua for microcontrollers) 0.4 released

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
darkore
Associate II
Posted on May 17, 2011 at 09:55

Hi,

eLua is an effort to bring the Lua programming language in the embedded world (MCUs). It is meant to be a complete MCU development environment. It currently runs on a number of ARM variants, as well as Cortex (and i386 as a proof of concept). Version 0.4 was just released, this is the changelog:

* Added support for LPC2888 (preliminary)

* Added PWM module

* New samples: TV-B-Gone (power off your TV), piano (play piano from your PC keyboard), pwmled (fade led on/off), all based on the new PWM module

* Added support for multiple memory spaces (this can be used to take advantage of both the internal CPU RAM and external RAM chips on boards that have external RAM)

* Autorun: if ''autorun.lua'' is found in the filesystem, it is executed before starting the shell

* Added ''pack'' (binary data packing/unpacking) and ''bit'' (binary operations) modules

* Build system updated, easier to use, now it knows how to handle ''boards'' as well as CPUs

* Modified the existing platform modules to take less RAM and to report an error when an unavailable resource is requested

* Project documentation updated

For more information visit the project homepage at

http://elua.berlios.de

Thanks,

Bogdan