cancel
Showing results for 
Search instead for 
Did you mean: 

[ANN] eLua 0.8 released

darkore2
Associate II
Posted on February 02, 2011 at 18:19

We are proud to annunce the release of 

http://www.eluaproject.net/

 v0.8

eLua is an effort to expand the presence of the Lua programming language in the embedded world, especially on microcontroller-based platforms. It is meant to be a complete MCU development environment. It currently runs on a number of ARM variants (including Cortex-M3), AVR32 (and i386 as a proof of concept).

The main changes from v0.7 are:

* Added the RFS (Remote File System), a new file system which allows sharing

a directory on the PC with the eLua board.

* Added a serial multiplexer which allows using more virtual serial ports over a single 

physical UART connection.

* Added Lua and C interrupt handlers support.

* Added linenoise support (eLua and Lua shell command line history and navigation)

* Added generic I2C support and docs

* Added hardware flow control and runtime configurable buffers for UARTs.

* Added support for new boards: mbed, EVK-1101, Mizar32, EK-LM3S1968

* Added SPI and SD/MMC support for EVK1100 and EVK1101 (AVR32) 

* Added I2C support for STR-E912 (STR912) 

* Added support for require() and autorun from SD/MMC

* Added external memory support for STR912

* Added long filename support for SD/MMC

* Added version() function to elua module

* Added RTC (real time clock) platform specific support for str9

* Added support for AsciiDoc in the doc builder

* Tutorials and new projects added to the eLua User Labs wiki

* Demo files were moved out of the distro to 

http://wiki.eluaproject.net/Projects

http://www.eluaproject.net/

* eLua wiki:        

http://wiki.eluaproject.net/

* Mail list:           

https://lists.berlios.de/mailman/listinfo/elua-dev

http://builder.eluaproject.net/

* Issue tracker:  

http://tracker.eluaproject.net/

* Other:             

http://www.eluaproject.net/en_comunity.html

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0