cancel
Showing results for 
Search instead for 
Did you mean: 

Again on watchdog in ST7lite29

ciccio
Associate II
Posted on May 06, 2009 at 06:42

Again on watchdog in ST7lite29

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
ciccio
Associate II
Posted on May 04, 2009 at 12:29

Hi,

I use ST7lite29 with internal oscillator.

My options bytes are:

Write Protection: OFF

Read Out: ON

SEC: 4K

OSCRANGE: Reserved

WDG_HALT: not reset in halt

WDG_SW: Software

LVD: medium

OSC: RC oscillator ON

PLL Enalbled and X8

Programmer: Indart STX

With this setting the watchdog don't work. :-[

If I setting:

OSCRANGE: MP:2-4MHz work!!! :D

Question:

is it correctly setting ''MP:2-4MHz'' when I use internal OSC?

What's I must select?

Thanks

wolfgang2399
Associate II
Posted on May 06, 2009 at 06:42

Hi Cicciounico,

in my opinion ''reserved'' means reserved for further application and should not be used.

Have a look at chapter 15 DEVICE CONFIGURATION:

Note: When the internal RC oscillator is selected,

 

the OSCRANGE option bits must be kept at their

 

default value ...

The default value for OSCRANGE is 111 = External Clock Source: CLKIN at PB4.

In my application it works fine with this setting.

Regards,

WoRo