cancel
Showing results for 
Search instead for 
Did you mean: 

ADC analog watchdog

vincentchoplin9198
Associate
Posted on February 15, 2013 at 08:07

I want to use ADC in AWD-Mode. This means the ADC shall generate an interrupt when a threshold at port 4.0 is exceeded. But I do not get it to run.

If I read ADC_DR0 correct data are read from analog input channel 0.

In ADC_CR I set the bits 9(AWDI), 4(CONT), 1(POR), 0(STR).

I set ADC_CCR to 0x0002 and ADC_HTR to the required threshold.

The ADC_CRR register does not change when the threshold is exceeded and the AWD-bit in ADC_CR is not set.

Does anyone has an idea whats wrong and does anybody got the AWD to run?

Thanks in advance

Pedro
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0