cancel
Showing results for 
Search instead for 
Did you mean: 

About DEBUG PROTECTION of str7

shangdawei1
Associate II
Posted on January 25, 2006 at 06:09

About DEBUG PROTECTION of str7

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
shangdawei1
Associate II
Posted on January 18, 2006 at 02:06

in FLASH PROGRAMMING REFERENCE MANUAL V 3.0

3.2 DEBUG PROTECTION

If bit DBGP of FLASH_NVAPR0 is programmed at 0, the device becomes Debug protected:

debug features JTAG pins and Flash SystemMemory mode are disabled.

Is External Memory boot mode enabled or disabled after Debug protected ?

if it is Enabled, When Boot from External Memory, Flash B0 and B1 can be readed out via program in External Memory ?

shangdawei1
Associate II
Posted on January 24, 2006 at 09:37

Quote:

On 20-01-2006 at 09:15, Anonymous wrote:

Is this information in the Reference Manual?

I have not found it in the Reference Manual.

has anybody found it ?

shangdawei1
Associate II
Posted on January 25, 2006 at 06:09

Quote:

On 24-01-2006 at 14:15, Anonymous wrote:

Hi,

I confirm this for you ''When the Debug Access Protection is activated for the Flash memory, RAM and EXTMEM boot modes are no longer available.''

This info is not yet in the reference manual.

Regards.

Thx, RISC !