cancel
Showing results for 
Search instead for 
Did you mean: 

A question about clock specification

daweiy
Associate II
Posted on April 19, 2006 at 08:17

A question about clock specification

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
daweiy
Associate II
Posted on April 19, 2006 at 04:48

Hello Moderaters,

I have a question about register RCCU_PLL1CR's bit6, FREF_RANGE. In specification, '1' indicates the input frequency, CLK2, should greater than 3MHZ, '0' means CLK2 from 1.5MHZ to 3MHZ.

In my test board, processor is STR710FZ2, external CK is a 4MHZ crystal, I set this bit to '1' and RCCU_CFR's bit15, div2, is reset value '1'. This means CLK2 is 2MHZ, bit 'FREF_RANGE' should be '0', the PLL1 works well. But my PLL1 works well with this bit, 'FREF_RANGE', is '1'.

Until now all good, but is there any potential problems with this kind of setting?

Could anyone answer this question?

Thanks.

Dawei