2006-02-17 06:28 AM
2011-05-17 03:10 AM
Hello
I have a problem with ports A & B when I'm running it on the DK3400. The attached program is a timer2 interrupt that toggles all PORTA from 0 to 1 .On the main I'm writing 0 and one to PORTA and it changes states. But when I'm running the program and tries to toggle PORTA it is stuck in one state and doesn't toggle. Can you ,please, give me a solution. Thanks Amir