cancel
Showing results for 
Search instead for 
Did you mean: 

VL53L1 underwater use / experiences?

Stefan Hamminga
Associate III
Posted on April 24, 2018 at 13:46

I understand the older vl6180x works underwater, but I could not find any information regarding the VL53L1. Anyone tried it? If so, how well does it work?

I'm looking mainly for proximity detection / distance measurement, but limited gesture/ motion detection would be a neat bonus.

#vl53l1
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
John E KVAM
ST Employee
Posted on May 02, 2018 at 00:04

The parts themselves have to be protected from the environment. But to a certain extent the light does go through water. Actually water absorbs 940nm light, so the max distance for the VL53L0x and VL53L1x will be cut down. But the max range is 2meters and 4 meters respectively. So please go ahead and try it. If you account for the speed of light through water, you should get a fine answer.


If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.