cancel
Showing results for 
Search instead for 
Did you mean: 

Using a STEVAL-MKI197V1 with a Nucleo-64 but without an expansion board

paul19
Associate III

I need to use a gyroscope with my Nucleo-64 board, but the gyroscope needs to stand apart (i.e. at the end of a cable). Is the STEVAL-MKI197V1 a good match? Can I connect it directly to my Nucleao-64 with a SPI cable, *without* using an expansion board? (such as X-NUCLEO-IKS01A1, X-NUCLEO-IKS01A2, X-NUCLEO-IKS01A3, X-NUCLEO-IKS02A1).

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Bruno_ST
ST Employee

Hello @paul19​ 

Yes there is no problem to connect it through cables instead of the easy plugin Arduino connector.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Bruno_ST
ST Employee

Hello @paul19​ 

Yes there is no problem to connect it through cables instead of the easy plugin Arduino connector.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

paul19
Associate III

Thanks @Bruno_ST. It works well indeed.

For reference, the SPI connection can be found here.