cancel
Showing results for 
Search instead for 
Did you mean: 

Recovery of Standby Mode in LIS3DH + STM32L072

Recovery of Standby Mode in LIS3DH + STM32L072

I am developing using LIS3DH + STM32L072 now.

I think that I want to restore with WKUP (PA0) of STM32L072 by INT1 when it enters Standby Mode and exceeds the threshold set to LIS3DH.

However, I will not return.

The settings are described below.

STM32L072

Setting of Standby Mode

void Enter_Standby_HAL (void)

{

__HAL_RCC_PWR_CLK_ENABLE ();

 HAL_PWREx_EnableUltraLowPower ();

 HAL_PWREx_EnableFastWakeUp ();

 if (__ HAL_PWR_GET_FLAG (PWR_FLAG_SB)! = RESET) {

__HAL_PWR_CLEAR_FLAG (PWR_FLAG_SB);}

HAL_Delay (5000);

HAL_PWR_DisableWakeUpPin (PWR_WAKEUP_PIN1);

 __HAL_PWR_CLEAR_FLAG (PWR_FLAG_WU);

 HAL_PWR_EnableWakeUpPin (PWR_WAKEUP_PIN1);

 HAL_PWR_EnterSTANDBYMode ();

while (1)

{

}

}

WKUP Pin setting

void Set_WkupPin1 (void)

{

GPIO_InitTypeDef initStruct = {0};

__HAL_RCC_GPIOA_CLK_ENABLE ();

 initStruct.Mode = GPIO_MODE_INPUT;

 initStruct.Pull = GPIO_PULLDOWN;

 HW_GPIO_Init (GPIOA, GPIO_PIN_0, & initStruct);

}

Setting of LIS3DH

CTRL_REG1 = 0x1F

CTRL_REG2 = 0xF9

CTRL_REG3 = 0x40

CTRL_REG4 = 0x00

CTRL_REG5 = 0x00

CTRL_REG6 = 0x00

INT1_THS = 0x03

INT1_DURATION = 0x00

INT1_CFG = 0x2A

For the beginners, I could not identify what was the cause.

Please tell me if you understand.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0