2016-05-23 6:18 PM
Hi all,
I recently designed a new PCB board for the LSM303DLHC Tilt-compensated compass ( please see attachment). I soldered everything onto the board and connected it to the microcontroller to test it, the raw data obtained from the sensor fluctuated and never went into the stable state. I am pretty sure the software that talk to the sensor is 100% working as I also tested with a sensor dev kit purchased from adafruit . so I just wonder if there is something wrong with my design. #pcb-guidelines