cancel
Showing results for 
Search instead for 
Did you mean: 

No Range or Raw Value

tekochip
Associate II
Posted on June 10, 2014 at 18:20

I am using a VL6180 as a proximity detector.  I am able to communicate the part without any issue, but when I read the

RESULT__RANGE_VAL register or

RESULT__RANGE_RAW

I only read 0xFF with no target and 0x00 with a target in any position.  I measured the current from the device and I can see that it is performing ranging at the rate I requested because I can see a spike in current draw that is proportional in length to the distance from my target, but the value in the result register does not change.  Other registers do show a change with target distance, but not the two result registers, so I�m sure I�m not setting something up right.

The only register altered from default is SYSRANGE__INTERMEASUREMENT_PERIOD, which I have at 10 for 100ms, and I do see a range measurement every 100ms.

#proximity-sesor #vl6180
This discussion is locked. Please start a new topic to ask your question.
11 REPLIES 11
heri
Associate II
Posted on February 25, 2015 at 13:22

What is the tuning settings that is not being completely loaded into the VL610X?

Is it this lists?

WriteByte(RegAddr, data)

WriteByte(0x0207, 0x01);

WriteByte(0x0208, 0x01);

...

I am facing approximately same problem.

heri
Associate II
Posted on February 26, 2015 at 12:32

OK, I got it. It works fine now.