cancel
Showing results for 
Search instead for 
Did you mean: 

MEMS barometer

reineking
Associate II
Posted on August 22, 2013 at 00:23

I'm using a LPS331 in a prototype. The datasheet does not give any timing information other than one can select the output data rate. What are the timing values for SPI such as max clocking frequency, etc. I search ST site and could not find any other information that would help. For I2C it says it complies with fast mode (400kHz) but nothing for SPI.

Thanks,

Tom

#mems-barometer
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Marco VENERI
ST Employee
Posted on August 23, 2013 at 16:42

Please note that this forum is specifically for MEMS Microphones and not for generic MEMS sensors. Anyhow, the LPS331AP max SPI clock frequency is 10MHz.