cancel
Showing results for 
Search instead for 
Did you mean: 

LIS3DH click and double click configuration

ksrgopinath
Associate
Posted on July 05, 2012 at 14:55

The original post was too long to process during our migration. Please click on the attachment to read the original post.
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
ksrgopinath
Associate
Posted on July 10, 2012 at 13:00

Hi guys,

          I have found the solution for this.In the application note CTRL_REG3 is metioned as the register to configure interruppt on INT1 pin but the correct configuration is use CTRL_REG6 bit 7 and bit 6(I2_CLICKen and I2_INT1) will enable tap and double tap interruppts on INT2 pin.(Tip:for tuning increase sampling rate (CTRL-REG1) increase time-limit value).

rasimoguzturk
Associate III
Posted on November 07, 2012 at 10:38

hi sri,can you post your I2C read write functions if possible?