2019-01-21 6:54 AM
I have prepared an application in which I am reading accelerometer x,y,z axis data from its registers @every 2 sec. Now what i observed is that if I keep my board at stable position without disturbing board or any surroundings still I see some spike value in one of the axis data. I have kept a threshold value for each axis.
Now due to this spike one of the axis crosses the threshold value. I do not understand that in idle position why such spike is observed.
If required I can share my application in which I have configured the registers at Init time and using X,Y,Z axis registers to read.
Please guide me in this issue.
Thank You,
Arjav Parikh
2019-01-21 7:03 AM
Compared with a known-working reference device (accelerometer) ?
Does the spike move with the axis when you turn the MEMS board ?
Tried a different environment (place) ?
In other words, what if the spike is real ?
2019-01-21 8:50 PM
Hi AvaTar,
Thank You for your response.
Please find answers inline:
Compared with a known-working reference device (accelerometer) ?
Ans: No. I don't have any working reference board for LIS3DH. I am using it with QCOM APQ8009 SOC.
Does the spike move with the axis when you turn the MEMS board ?
Ans: When I move the board I see the change in Axis value as expected. But in ideal condition (when not rotating the board) also I see spike and then again it gets back to normal.
Tried a different environment (place) ?
Ans: No. What ideal environment shall I check this.
In other words, what if the spike is real ?
Ans: As per my project use In ideal position spike is not expected because in application I have taken a threshold value such that if threshold value is crossed then I will consider it as a theft detection case. So I need to eliminate the spike in ideal condition.
I have not configured Interrupts in LIS3DH. I am just reading the axis values from its registers.
Please let me know in case of any additional information required from my end.
2019-01-21 10:31 PM
> Ans: No. I don't have any working reference board for LIS3DH.
> Ans: No. What ideal environment shall I check this.
Have you considered the "spikes" as measurement of real events in your environment ?
Perhaps large machinery, transportation, or mining ?
Avoid hunting phantoms.
If the downward pointing axis measures 1g, and the measurement follows when turning the accelerometer, you are fine.
2019-01-21 10:57 PM
> Have you considered the "spikes" as measurement of real events in your environment ?
Ans: Yes. I am continuously reading value from registers.
Current environment scenario is accelerometer is mounted on embedded board within room temperature.
Please find below detail for current issue w.r.t application:
At boot time when my accelerometer application starts, I have configured below registers:
Init() {
FIFO_CTRL_REG = 0x80 (Enable Stream Mode)
CTRL_REG0 = 0x90 (SDO/SAO Pull Up Disconnected for I2C)
CTRL_REG1 = 0x77 (ODR is 400 Hz H-RES Mode,X-Axis En, Y-Axis En, Z-Axis En)
CTRL_REG4 = 0x08 (H-RES Mode)
CTRL_REG5 = 0x40 (FIFO ENABLED)
}
Read() /* This function is called every 2 sec */ {
Read : x_axis_lsb = OUT_X_L, x_axis_msb = OUT_X_H
x_axis = (x_axis_msb << 8 | x_axis_lsb);
Read y_axis_lsb = OUT_Y_L, y_axis_msb = OUT_Y_H
y_axis = (y_axis_msb << 8 | y_axis_lsb);
Read z_axis_lsb = OUT_Z_L, z_axis_msb = OUT_Z_H
z_axis = (z_axis_msb << 8 | z_axis_lsb);
}
a. In read function during idle position I get below values for each axis:
x-axis : 0x40 / 0x0, y-axis : 0x40 / 0x0, z-axis : 0x40 / 0x0
b. In same position (no orientation/position change) after some time I get below values:
x-axis : 0xC040 / 0xFFC0, y-axis : 0xC0 / 0x100, z-axis : 0x5780 / 0x1AC0
My expectation is that in ideal condition I should always get values mentioned in case a. Am I doing something wrong while configuring registers?