cancel
Showing results for 
Search instead for 
Did you mean: 

How to convert the value to Temperature and Humidity for HTS221?

x22819
Associate
Posted on August 29, 2014 at 11:28

I have using HTS221 , and I have get the value from HTS221 via I2C.

The value is like the following:

Read HTS221 CTRL_REG1: 0x20 value is 0x81

Read HTS221 CTRL_REG2: 0x21 value is 0x0

Read HTS221 CTRL_REG3: 0x22 value is 0x0

Read HTS221 STATUS_REG: 0x27 value is 0x0

Read HTS221 HUMIDITY_OUT_L: 0x28 value is 0xAA

Read HTS221 HUMIDITY_OUT_H: 0x29 value is 0x10

Read HTS221 TEMP_OUT_L: 0x2a value is 0xB5

Read HTS221 TEMP_OUT_H: 0x2b value is 0x0

Read HTS221 T0_degC_x8: 0x32 value is 0xBF

Read HTS221 T0_degC_x8: 0x33 value is 0xBF

Read HTS221 T1/T0 msb: 0x35 value is 0x4

Read HTS221 T0_OUT-3C: 0x3C value is 0x0

Read HTS221 T0_OUT-3D: 0x3D value is 0x0

Read HTS221 T1_OUT-3E: 0x3E value is 0x0

Read HTS221 T1_OUT-3F: 0x3F value is 0x0

It seems the data of the temperature and the Humidity is like the following:

Read HTS221 HUMIDITY_OUT_L: 0x28 value is 0xAA

Read HTS221 HUMIDITY_OUT_H: 0x29 value is 0x10

Read HTS221 TEMP_OUT_L: 0x2a value is 0xB5

Read HTS221 TEMP_OUT_H: 0x2b value is 0x0

And it give some example in data sheet like the following:

Step 1: Temperature conversion from ADC_OUT (LSB) to �C

Step 1: Linear interpolation (example)

Table 20. Step 1: Linear interpolation to convert LSB to �C

Conclusion: current temperature is 15 �C.

Input Temperature LSB (ADC) Output Temperature (DegC)

T0_OUT = 300 (T0 msb U T0_degC_x8) = 80�C => 80/8 = 10.0 �C

T_OUT = 400 T_degC_x8 =120 [interp.] =>T_degC=120/8 = 15.0 �C

T1_OUT = 500 (T0 msb U T0_degC_x8) = 160�C => 160/8 = 20.0 �C

But I still inderstand how to covert the above data of the temperature and the Humidity to 

actual temperature and Humidity ?

Does someone can teach me ?

Thank in advance.

#hts221 #temperature-sensor
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
jayesh1
Associate
Posted on September 22, 2015 at 08:23

Hi martin,

Read the values of the following register listed below,

T_OUT 

T0_T1_MSB 

T0_degC_x8 

T1_degC_x8 

temp_T0_degC 

temp_T1_degC 

temp0_out 

temp1_out 

After getting all this values just put in below formula and get temp.

T_DegC = (temp_T0_degC + (temp_out - temp0_out) * (temp_T1_degC - temp_T0_degC) / (temp1_out - temp0_out));