• Images in Public (D.Botelho)
  • My Images for D.Botelho

My Images for D.Botelho

  • Albums
  • All Images
Image Options
  • Flag Image for Review
  • Bookmark
  • Subscribe to RSS Feed

Album: Public (D.Botelho)

by D.Botelho
Fig. 4 - NUCLEO-G0B1RE
Fig. 5 - X-NUCLEO-DRP1M1
Fig. 6 - STM32 Project creation
Fig. 7 - Enabling the UCPD1 peripheral configuration
Fig. 8 - Enabling the DMA Channels for the UCPD1
Fig. 9 - Enabling the USBPD Middleware
Fig. 10 - Enabling the FreeRTOS Middleware
Fig. 11 - Enabling the I2C
Fig. 12 - Enabling the ADC
Fig.13 - Opening the Select Components menu
Fig. 14 - Enabling the X-CUBE-TCPP
Fig. 15 - Enabling the X-CUBE-TCPP
Fig. 16 - Adjusting the Clock Configuration
Fig. 17 - Increasing the minimum heap
Fig. 18 - Adjusting the code generation settings
Fig. 19 - Enabling and configuring the USART2
Fig. 20 - Activating the USART2 interrupt
Fig. 21 - Adding the USART2 TX DMA channel
Fig. 22 - Enabling the Uart Trace Source
Fig. 23 - Enabling the Trace at USBPD Middleware
Fig. 24 - Enabling the GUI Interface
Fig. 25 - Enabling the USB Peripheral
Fig. 26 - Selecting the USB Device Class
Fig. 27 - Enabling the USB Support at USBPD Middleware
Fig. 28 - Generating the code
Fig. 29 - Warning during code generation
Fig. 30 - Selecting the Virtual COM Port at STM32CubeMonitor-UCPD
Fig. 31 - Selecting the UCPD Port at STM32CubeMonitor-UCPD
Fig. 32 - STM32CubeMonitor-UCPD Interface
Fig. 33 - Virtual COM Port recognized in Device Manager
Fig. 34 - Virtual COM Terminal showing the messages
Fig.1 - NUCLEO-C031C6
Fig. 2 - Enabling the SPI - STM32CubeIDE
Fig. 3 - SPI pins at NUCLEO-C031C6 schematics
DBotelho_3-1733268839379.png
Fig. 4 - Enabling the Timer - STM32CubeIDE
DBotelho_5-1733268886201.png
Fig. 5 - Generating the code - STM32CubeIDE
Fig. 6 - SPI Transmission - Logic 2
Fig. 7 - Pins to be shorted at NUCLEO-C031C6
Fig. 8 - SPI Transmission and Reception - Logic 2
Fig. 9 - Reception buffer during debug - STM32CubeIDE
Fig. 10 - Sending a command at SPI - Logic 2
Fig. 11 - Sending a command at SPI - Logic 2
Fig. 12 - Reconfiguring the timer - STM32CubeIDE
Fig. 13 - SPI with pulsed chip select - Logic 2
Fig. 14 - SPI with Chip Select with zoom - Logic 2
DBotelho_0-1743597273023.png
DBotelho_13-1733172210214.png
Previous
Fig. 30 - Selecting the Virtual COM Port at STM32CubeMonitor-UCPD
Next
Added ‎2024-12-02 12:43 PM
0 Kudos
Fig. 30 - Selecting the Virtual COM Port at STM32CubeMonitor-UCPD