• Images in Public (Mohammad MORADI ESFAHANIASL)
  • My Images for Mohammad MORADI ESFAHANIASL

My Images for Mohammad MORADI ESFAHANIASL

  • Albums
  • All Images
Image Options
  • Flag Image for Review
  • Bookmark
  • Subscribe to RSS Feed

Album: Public (Mohammad MORADI ESFAHANIASL)

by Mohammad MORADI ESFAHANIASL
Setting the visual element of the flex button to 0
TouchGFX Board Setups
TouchGFX Board Setups
STM32U5A9J DK board setup
Bill of Material for STM32U5G9J-DK2
Touch controller code used in STM32U5G9J-DK2
STM32H735G-DK Board Specific Demo
STM32H7B3I DK Board Setup
JPEG settings in MDMA
JPEG and MDMA interrupt
STM32H735G-DK TouchGFX Board Setup
Import GUI.png
Adding Input_Test pin
Project running on the board
Demos available in the TouchGFX designer
Selecting the desired demo/example
Selecting the desired TBS
Importing GUI
Available TBSs for STM32F469
NUCLEO-WB55RG TBS
Buffer Location configuration
STM32H735G-DK TouchGFX Board Setup
.ioc file
Enabling I2C and generating code
NUCLEO TBSs
TBSs using SPI display interface
STM32F746G-Disco Board Specific Demo
TBS for STM32F746G Disco
FreeRTOS settings
main_user.c
Modal Window Example
vShortEn.png
Includes in STM32CubeIDE.png
Board Setup for STM32H7S78 DK
Board Setup for STM32U5G9J DK2
TBS for STM32H7B3I-Eval
TBS for STM32H7S78-DK
RGB888 + Double Framebuffer
RGB565 + Single Framebuffer
RGBA2222 + Single Framebuffer
Understanding Application Structure example
NUCLEO-H503RB + GFX01M2
Display Orientation Settings
STM32H7B3I-DK Board Setup
SDRAM section
Simulator showing the QR Code
Project running on STM32F429I-Disco
TBS for STM32H750B-DK
TouchGFX Demo 5
Display dimensions
By Allocation.png
Previous
Buffer Location configuration
Next
Added ‎2024-07-12 2:59 AM
0 Kudos
Buffer Location configuration
Posted in: Re: Video decoding for STM32H7B3L. - ( ‎2024-07-12 3:22 AM )