• Images in Public (Denise SANFILIPPO)

Images in Public (Denise SANFILIPPO)

  • Albums
  • All Images
Album Privacy: Public
  • « Previous
    • 1
    • …
    • 36
    • 37
    • 38
    • …
    • 41
  • Next »

Public (Denise SANFILIPPO)

  • Picture24.png
  • Picture25.png
  • Picture26.png
  • Figure 23:  The MCU stop block appears inside the MCU library
  • Picture28.png
  • Picture29.png
  • Picture31.png
  • Figure 27: Import the project inside STM32CubeIDE
  • Figure 28: Select root directory to your STM32U3 firmware location
  • Figure 29: Select the build configuration you want to use
  • Figure 29:
  • Figure 6: MEMS Studio - AlgoBuilder - Blocks
  • Figure 7: MEMS Studio - AlgoBuilder Evaluation
  • Figure 8: MEMS Studio - AlgoBuilder Evaluation - Save to File
  • Figure 10: MEMS Studio - Advanced Features - MLC - ARFF generation
  • Figure 11: MEMS Studio - Advanced Features - MLC - Decision tree generation
  • Figure 12: MEMS Studio - Advanced features - MLC - Config generation
  • Figure 14: AlgoBuilder - Adding FSM/MLC blocks
  • Figure 15: AlgoBuilder - Adding Value block
  • Figure 16: MEMS Studio - AlgoBuilder Evaluation - The package is still
  • Figure 17: MEMS Studio - AlgoBuilder Evaluation - The package is not in an upright position
  • Figure 18: MEMS Studio - AlgoBuilder Evaluation - The package is moving
  • Figure 19: MEMS Studio - AlgoBuilder Evaluation - The package is shaken
  • Figure 20: Create a “Custom library” called “MCU”, and inside it a custom block called “MCU Stop”
  • Figure 21: Set the required info, inputs, outputs, and the code to enable MCU stop block
  • Figure 22: Simple C code can be put in the function block, to enable stop mode
  • Figure 23:  The MCU stop block appears inside the MCU library
  • Figure 24: The block tree is completed
  • Figure 25: AlgoBuilder Evaluation - Custom layout
  • Figure 26: Select the workspace to your firmware location