cancel
Showing results for 
Search instead for 
Did you mean: 

STML011K4 Stopmode consumes too much current.

SPlat.1
Associate

Hello,

Running my program on the STML011k4 consumes about 50mA, when in stopmode this drops down to about 40 mA. I know the stopmode does still power the RAM, but 40mA is way too high according to the datasheet.

Another thing I find odd is that the LEDs on the board don't turn off, and I find this weird because the LEDs consume a lot of power, so you would expect that they get turned off when the device is put into stopmode.

I use the following HAL function to enter the stopmode: HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI);

I also tried entering stopmode by setting the registers myself, but this makes no differece in current consumption.

I use an external interrupt to wake the device up out of the stopmode, this seems to work fine.

Also I am quite sure the core gets powered off, because I can not debug when HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI); is executed.

All my unused pins are set to analog.

Could somebody help me out here?

Kind regards,

Sjoerd

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0