cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-BCN002V1 Sensor Demo Project Code Walk-through

garyng98
Associate

Dear all, I am new to STEVAL-BCN002V1.

I will like to inquire if there is any workshop presentation materials or materials which can explain to me the code walk-through for the entire STEVAL-BCN002V1.

As I will only use acclerometer and pressure sensor to get free-fall function, step counter, acitivites recongition.

Also, I will like to ask why am I able to add the customised C code which I had build using algobuilder to the whole project.

Please teach.

Best Regards

Gary

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Winfred LU
ST Employee

Hi Gary,

Please start from: STEVAL-BCN002V1B QUICK START GUIDE

https://www.st.com/resource/en/product_presentation/steval-bcn002v1b_quick_start_guide.pdf

Then, in after unpack the DK, there is a folder Docs with documents for your needs.

There are also user manuals or application notes available on ST web site:

https://www.st.com/en/wireless-transceivers-mcus-and-modules/bluenrg-1.html

Yes. You are able to customized firmware (C source code) for the projects.

Thank you.

Best Regards,

Winfred