cancel
Showing results for 
Search instead for 
Did you mean: 

ST60A3H1 underwater performance?

StefanH
Associate III

The ST60A3H1 looks very interesting. While I understand an NDA is required for access to the complete details on this solution, would it be possible to say if it works underwater as communication between ROV modules?

Scenario:
IC A | 1mm air or mineral oil | 5mm plastic | ~5-10mm (sea) water | 5mm plastic | 1mm air or mineral oil | IC B
Would this work at all? Even when only working at lower speed (for example USB FS / 12Mbit) this would be interesting.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

After consultation with our specialists, we regret to inform you that the 60 GHz carrier frequency used is not suitable for underwater transmissions because it is completely blocked. This means that no meaningful transmission is possible with this frequency, not even at lower data rates.

Hope that answers your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

After consultation with our specialists, we regret to inform you that the 60 GHz carrier frequency used is not suitable for underwater transmissions because it is completely blocked. This means that no meaningful transmission is possible with this frequency, not even at lower data rates.

Hope that answers your question?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.