cancel
Showing results for 
Search instead for 
Did you mean: 

SPWF04 - Station Disassociated: ... :1

Mareike H
Associate II
Posted on September 01, 2017 at 12:24

I have some trouble with getting disassociated because I reload one of my pages very often to get the newest SSI information on the webpage from the microcontroller. I get the message: '+WIND:72:Station Disassociated: ... :1'.

I am using the SPWF04 in MiniAP mode and with firmware 1.0.0

For testing I am using a html page with:

<body onload='window.location.reload(false)'>

In the user manual I found the variable wifi_txfail_thresh which is for the maximum number of lost packets before disassociation. When I set it to a higher number I don't get disassociated so fast. When I set it to 0 or 1 I get disassociated very fast.

With the standard value 5 it takes between 1 and 15 minutes after a reset until disassociation.

My question is: Is it possible to disable the disassociation function? I don't want to be disassociated no matter how many packets are lost...

Thanks and regards

Mareike
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0