Skip to main content
Grigori
Associate II
September 25, 2015
Question

SPWF01SC.21 module AT-commands library

  • September 25, 2015
  • 13 replies
  • 2426 views
Posted on September 25, 2015 at 13:41

Hi,

Is there any reference AT-commands library written in C for SPWF01 modules? Googling didn't help. Target OS is FreeRTOS, but generic C library is acceptable.

I know, I can write it using state machines etc. It will take time. I believe many of you have already implemented something related.

I would also glad to hear any clues on generic AT-commands libraries which could be easily extended for this module.

They should support at least following functionality:

- data and command states

- async status messages from modem

Could also somebody answer two additional questions:

- if there any status messages while module is in data mode? So, should I check RX buffer in data mode for something like ''+WIND:''?

- what happens in case of closed socket on remote end or lost network? Will module return to command mode itself?

Answer to these additional questions would help in implementing own state machine.

Thank you.

#spwf #spwf01s-wifi #spwf01
    This topic has been closed for replies.

    13 replies

    benny23
    Associate II
    November 17, 2015
    Posted on November 17, 2015 at 11:06

    Hi Jerry,

    Thank you very much.

    Regards.

    Benny

    benny23
    Associate II
    November 27, 2015
    Posted on November 27, 2015 at 09:03

    Hi Jerry,

    Does ST have any plan to provide a SPWF01 firmware library for STM8 like for STM32? Or, to release application notes to guide the STM8 users?

    Regards.

    Gerardo GALLUCCI
    ST Employee
    November 27, 2015
    Posted on November 27, 2015 at 09:16

    Hi Benny,

    I don't think so. Porting from STM32 to STM8 should be an easy task.

    I will share updates if/when available.

    j