2016-05-29 10:10 PM
I have our BlueNRG device set up to use a fixed pin for pairing.
I am able to successfully pair with Apple iOS decvices and windows phone when I enter the correct PIN when prompted by the device. However when connecting to an Android device, the pairing always fails even though I enter the correct PIN when prompted. Using a packet sniffer I can see that the reason for failing is 0x04 (The confirm value does not match the calculated compare value). I have tried with several different Android devices and versions including 4.4, 5.1 & 6.0 and I have the same issue with all of these. Has anyone successfully paired an Android device with BlueNRG using a PIN code? Regards Nick #bluenrg-pairing #android #android #bluenrg-pairing2016-11-29 8:58 AM
Hi Nick,
I have the same problem as you desctibed, did you find any solution to pair your android device to the bluenrg ? Thanks,MBR2016-11-30 9:35 AM
Hi guys,
I did have issues similar to you guys but I was entering the password as a hex value. Simple I know but may be the cause. I just got mine paired and will work on the comms tomorrow hopefully.2016-12-01 12:24 AM
....and as well as that I also noticed that rev6 of the User Manual (UM1686) doesn't provide the parameter details for the
aci_gap_set_authentication_requirement
comand.I retrieved theses settings from the rev3 document.Regards,codaci_gap_set_authentication_requirement
MITM_Mode
= 0x01
OOB_Enable
= 0
OOB_Data
= 0
Min_Encryption_Size
= 0x07
Max_Encryption_Size
= 0x
10
Use_Fixed_Pin
= 0
Fixed_Pin
= 123456 (decimal)
Bonding_Mode
= 1
aci_gap_set_authentication_requirement
2016-12-01 1:28 AM
Hi all,
i have successfully paired SPBTLE-RF with Android and iOS devices. result = self.aci_gap_set_auth_requirement( mitm_mode=MITM_PROTECTION_REQUIRED, oob_enable=bool(OOB_AUTH_DATA_ABSENT), oob_data=b'\x00'*16, min_encryption_key_size=MIN_ENCRY_KEY_SIZE, max_encryption_key_size=MAX_ENCRY_KEY_SIZE, use_fixed_pin=bool(USE_FIXED_PIN_FOR_PAIRING), fixed_pin=123456, bonding_mode=BONDING) I have reimplemented a pure python drivers for based on bluenrg dk ''2.0.2''. MicroPython v1.8.6-114-g8b82429-dirty on 2016-11-30; PYBv1.1 with STM32F405RG Type ''help()'' for more information. >>> from sensor_demo import SensorDemo >>> ble = SensorDemo() >>> ble.run() INFO:examples.sensor_demo current version 7.2c INFO:examples.sensor_demo #acc_serv_handle 000c INFO:examples.sensor_demo #free_fall_char_handle: 000d INFO:examples.sensor_demo #acc_char_handle: 0010 INFO:examples.sensor_demo #env_serv_handle 0013 INFO:examples.sensor_demo #temp_char_handle: 0014 INFO:examples.sensor_demo #press_char_handle: 0017 INFO:examples.sensor_demo gap_connection_complete_cb INFO:examples.sensor_demo gap_disconnection_complete_cb INFO:examples.sensor_demo gap_connection_complete_cb INFO:examples.sensor_demo gap_disconnection_complete_cb INFO:examples.sensor_demo gap_connection_complete_cb INFO:examples.sensor_demo gap_disconnection_complete_cb Regards, D.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.