cancel
Showing results for 
Search instead for 
Did you mean: 

Inquiry regarding PWM driving of Inductive Loads with VND5T100LAJ-E

Chiranjeevi9391
Visitor

Hello,

I am evaluating the VND5T100AJ-E for an automotive application where I need to drive a 24V contactor. My design requirement is i need to drive the IC through the PWM signal as input.

I have reviewed the datasheet but do not see explicit PWM frequency ratings. My concerns are:

  1. Does the VND5T100AJ-E support continuous PWM switching for an inductive load?

  2. If this device is not recommended for PWM, could you suggest a similar specification alternative part with the same specifications  that is specifically designed for PWM input @stmicro 

0 REPLIES 0