cancel
Showing results for 
Search instead for 
Did you mean: 

Incorrect BOM Values of X-NUCLEO-IDB04A1 BlueNRG Board

moataz
Associate
Posted on July 04, 2016 at 13:15

Hello Regarding BOM values of:

http://www.st.com/content/ccc/resource/technical/document/bill_of_materials/d7/c0/bb/6b/fd/17/42/16/x-nucleo-idb04a1_bom.pdf/files/x-nucleo-idb04a1_bom.pdf/jcr:content/translations/en.x-nucleo-idb04a1_bom.pdf

L4, the required value is 1.8pF however the part number GRM1555C1H180JZ01 indicates 18pF, which is correct?

C25, the required value is 1.2pF however the part number GRM1555C1H120JZ01 indicates 12pF, which is correct?

Thanks in advance.
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0