cancel
Showing results for 
Search instead for 
Did you mean: 

in L9950 ic i am unable to control the out11 ic

prabhu bhavikatti
Associate II
Posted on August 16, 2017 at 12:29

in l9950 ic all output enabling and disabling exept out11 pin how can configure them.

This discussion is locked. Please start a new topic to ask your question.
7 REPLIES 7
Ignazio Testoni
ST Employee
Posted on August 31, 2017 at 14:42

Hi

g.prabhu

,

Controlling OUT11 is not different that controlling other HS output like OUT7 to OUT

Please double check your SPI register configuration.

Best Regards.

Ignazio

Posted on September 01, 2017 at 12:19

All other high side switches are working properly only out11 is not working properly i checked my time 

Regards

Prabhu

Ignazio Testoni
ST Employee
Posted on September 06, 2017 at 11:08

Hello Prabhu,

once you have turned on OUT11, could you please read all register contents and provide it here?

Thank you.

Regards.

Ignazio

Posted on September 07, 2017 at 07:53

hi ignazio,

If i make only out11 high then out11 will high.if i make it low should make enable bit as low.

Thank you 

Regards

prabhu

Posted on September 08, 2017 at 00:10

I'm sorry Prabu,I don't understand really the problem.

Is OUT11 working properly or not?

Ignazio

Posted on September 12, 2017 at 08:49

Hi Ignazio,

OUT11 Pin is working and it is always High. I'm not able to make it Low. 

I need one more support regarding the varying the voltage levels 12V, 9V and 6V on the OUT Pins. Kindly help us how to do this. And is there any sample code or development platform available for this IC l9950 ?

Regards

Prabhu.

Posted on October 14, 2017 at 19:47

Hi Prabhu,

Is OUT11 always high even if loaded with some resistor value?

If is always ON and able to supply some loads, the IC could be damaged.

What do you mean by varying the output voltage of the OUT Pins?

Those outputs are High Side Drivers means that they bring out the Battery Level when active.

If the Battery level is 12V they will give you 12V ou output.

If you supply with 9V they will give you 9V and so on.

Ignazio