cancel
Showing results for 
Search instead for 
Did you mean: 

Does flash readout protection activation via bootloader protect SWD read as well on BlueNRG-232?

rds-tmeyer
Associate II

I have a BlueNRG2 firmware that includes critical application level encryption keys. It is flashed using the bootloader. If I activate the flash readout protection using the bootloader commands (0x82), is the flash protected from readout through SWD as well?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0