2015-11-17 10:10 AM
2015-11-18 7:20 AM
2015-11-19 6:33 AM
Thanks for the reply.
From another post I already knew the changes on fw 7.1 But with the help of another colleague I discovered that the problem was a too short time settings for HS_Startup_Time. It worked fine with the evaluation board, but with the new custom board, I had to change it to 1.4ms. Now the board is seen by other devices almost immediately and can exchange data with them. In the application notes, indeed was written that a too short time would make impossible to send/receive packet (even if it is not put in evidence enough in my opinion, I would suggest a troubleshooting or FAQ with the common mistakes on the IFR configuration)We’re moving the ST Community to a new platform to give you a better and more reliable community experience.