cancel
Showing results for 
Search instead for 
Did you mean: 

BlueNRG-MS Not advertising

KS.9
Associate II

I have created a project for STM32L452CE using CubeMX and added BlueNRG-MS package (Additional software component).

In the BlueNRG-MS package, I have selected the sensor demo application. Since our board is a custom board the pin configuration for BSP related components is changed accordingly. 

When the generated code is running I am getting the below logs which shows the successful initialisation of BLE stack and entry into General discoverable mode. 

But when I scan for the nearby devices through BlueNRG mobile application I am not able to find our device. But when BSP Button interrupt is generated the BSP LED is being toggled as per the implementation.

DEBUG Logs:

   

HWver 49

FWver 1813

BLE Stack Initialized.

SERVER: BLE Stack Initialized

Service ACC added. Handle 0x000C, Free fall Charac handle: 0x000D, Acc Charac handle: 0x0010

Acc service added successfully.

Service ENV_SENS added. Handle 0x0013, TEMP Charac handle: 0x0014, PRESS Charac handle: 0x0017, HUMID Charac handle: 0x001A

Environmental Sensor service added successfully.

General Discoverable Mode.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0