cancel
Showing results for 
Search instead for 
Did you mean: 

AutoReconnect Problem // SPBT3.0DP2

Thomas Obermeier
Associate II
Posted on January 29, 2018 at 21:11

Hi

I'm using the SPBT3.0DP2-Module to build a custom HID keyboard. Unfortunately, the module doesn't automatically reconnect to the host-device (for Testing my Win10 PC and Android Smartphone) after disconnection (switching off/on the host-device or BT-Module). I have to connect new, manually.

Here the used Commands: (UM2077-Manual):

AT+AB Reset
AT+AB Config DeviceName = MyDevice
AT+AB Config EnableHIDKeybd = TRUE
AT+AB Reset
AT+AB AutoReconnect enable
AT+AB AutoReconnectSetup 5 2000 // i want a reconnect all 5 Seconds�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

What did Iwrong? #spbt3.0dp2 #autoreconnect #bt-classic #hid #at-command
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
fatih erdogan
Associate
Posted on March 16, 2018 at 15:28

I have also this question STM. Please help us.

Is this possible that I can not reconnect because first i have started the connection from the PC (PC = Master) (SPBT = Slave). Then I want to do a Reconnection but my SPBT is still the slave and is usually not able to establish a connection? or is there any possibilty to do an autoreconnection?

Thanks!