cancel
Showing results for 
Search instead for 
Did you mean: 

ADC polling in Bluenrg1 - I am using ADC polling peripheral code in Bluenrg1 module.Code is working upto 100ms delay in SdkDelayMs(100); but as i increase delay 1000ms adc not reading values but code is running.

PMeth
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Winfred LU
ST Employee

I tested with a STEVAL-IDB008v2 (BlueNRG-2) with ADC polling project (SDK 3.1.0), and SdkDelayMs(1000) worked fine.

Note. The ADC in BlueNRG-2 is the same as the ADC in BlueNRG-1.