| Subject | Author | Posted | |
|---|---|---|---|
|
Hello everyone, I am working with an SPC58NH92C5RMI0X microcontroller using SPC5Studio v6.0 and th...
| 2025-08-07 11:53 AM | ||
|
Hi, Im new to SPC582 my issue is I need to enable ICU at eMIOS0 Channel 22 , I have enabled the pi...
| 2025-08-07 5:31 AM | ||
|
Dear ST Support Team, I hope you are doing well. Our team is currently working on a Mining Vehicl...
| 2025-07-26 10:48 PM | ||
|
Dear, I am trying to setup a channel of the EMIOS into DAOC mode. I walked through an example of u...
| 2025-07-25 7:02 AM | ||
|
I'm currently try to work with the SPC584B70E1. Debugging with the AEK-MCU-SPC5LNK with openOCD, i...
| 2025-07-22 12:07 AM | ||
|
Hello, I am trying to program the SPC563M64 microcontroller using the UDESTK programmer and UDE...
| 2025-07-21 5:51 AM | ||
|
I am currently working on configuring the ADC using the CTU module. However, I’m facing some issues...
| 2025-07-08 2:46 AM | ||
|
We are currently conducting CAN communication using the SPC584Bxx chip. We are trying to develop a ...
| 2025-07-07 1:58 AM | ||
|
I'm trying to connect to SR5E1-EVBE7000P using JLINK , but all methods failed. Here's what I tried
| 2025-07-03 3:04 AM | ||
|
我想要一个用于细微软件延迟的代码。我的 MCU SPC560B50L3,软件SPC560STUDIO。
| 2025-06-25 7:18 PM | ||
|
Hello everyone, I'm working with SPC58 microcontrollers and configuring 6 PWM channels using diffe...
| 2025-06-09 9:14 AM | ||
|
Just got an SPC560P-DISP and I'm following AN4487 Getting started instructions. I have the board co...
| 2025-06-05 11:28 AM | ||
|
For your information ,
The StellarStudio 7.2.0-JOURNEY version has been officially released for W...
| 2025-05-20 1:19 AM | ||
|
Dear Team,
I have some doubts about How to use SPC5 Studio Application for Enabling GPI...
| 2025-05-14 2:29 AM | ||
|
Hello, I'm using the SPC58NH-DISP board, and my application needs to preserve some variables across...
| 2025-05-01 4:11 PM | ||
|
Hallo, I tried to use the DSPI_0 interface with the transfer configuration as shown in the picture...
| 2025-04-23 4:36 PM | ||
|
I want to generate pwm signal with spc582B with out the signal directly to pin emios0 channel 11 (u...
| 2025-04-16 8:42 PM | ||
|
Hello, As part of a custom BMS project, I am trying to add a cyclic CAN Message Transmission funct...
| 2025-04-16 8:00 AM | ||
|
Hello, I just received a copy of the STEVAL-TTM005A. From the documentation, if I use a 5V power ...
| 2025-04-15 9:11 AM | ||
|
I’m trying to implement FOTA on SPC58NH, and changing the application start address is causing some...
| 2025-04-15 3:11 AM |