| Subject | Author | Posted | |
|---|---|---|---|
|
Good morning everyone, I'm here to ask for advice regarding the approach I want to take for enabli...
| 2024-12-23 12:38 AM | ||
|
Hello Everyone, I am working on a UVC project using the STM32U5G9ZJT6Q MCU, capturing 8-bit data v...
| 2024-12-17 1:27 AM | ||
|
Hello I'm developing RTOS environment of dual-core in STM32H757. Using the functions osThre...
| 2024-12-16 9:29 PM | ||
|
Hello STM Community!, I'm trying to implement USB CDC ACM in standalone mode(without using ThreadX...
| 2024-12-16 3:39 AM | ||
|
I recently began using the B-L462E-CELL1 module for IoT applications, connecting it to a Raspberry ...
| 2024-12-15 11:27 PM | ||
|
hi, im using stm32g474vet6 tim_bkin for pwm shutdown through external pin, when im normally using p...
| 2024-12-11 6:15 PM | ||
|
Hi everyone, I encountered a challenging issue while using GUIDRV_LIN_OSY_16 with STemWin on an ST...
| 2024-12-11 4:21 AM | ||
|
Hello, I am newbie and i have project with STM32F407G-DISC1 and PMOD I2S2. It generates two RNG va...
| 2024-12-07 8:56 AM | ||
|
Hi, I have an http web server running on a STM32U575. The system is reachable via USB over RNDIS. H...
| 2024-12-06 11:26 PM | ||
|
Dear all !
I in my project have 1 led was blink to know CPU still working, display TFT LCD ST7735...
| 2024-12-04 10:26 PM | ||
|
I am using a user defined diskio function (found online here https://github.com/kiwih/cubeide-sd-ca...
| 2024-12-02 7:01 PM | ||
|
FreeRTOS is not started, failed on configASSERT( ( portMAX_PRIGROUP_BITS - ulMaxPRIGROUPValue ) == ...
| 2024-12-02 4:10 AM | ||
|
Hi
Is there a plan to update the x-cube-freertos Kernel to 11.1.0?
Github repo: STMicroelectron...
| 2024-12-01 11:15 PM | ||
|
Hello ST Community, I’m working on a project where I initially developed software on the STM32H735...
| 2024-11-25 2:41 AM | ||
|
Good afternoon, We use ThreadX in conjunction with TouchGFX. As debugger we use ST-Link/V2...
| 2024-11-24 10:44 PM | ||
|
Hello, trying to port Miro Samek's example: https://github.com/QuantumLeaps/FreeACT - into my n...
| 2024-11-24 3:26 PM | ||
|
Hi, my goal was to play some .wav audio files from an external SD card using the onboard DAC and an...
| 2024-11-23 5:02 PM | ||
|
Hi All I have a problem with a ThreadX-based project on a Nucleo H563ZI board when using a mutex. ...
| 2024-11-20 9:28 AM | ||
|
Hi,
I have a custom PCB where I am attempting to bootload an STM32G071CBU6 (using an STM32U575). ...
| 2024-11-14 7:16 PM | ||
|
Hello everyone and thank you for your help, I am being using the STM32F746G-Discovery Board for a c...
| 2024-11-10 11:14 PM |