cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to include header file

Rajendra Bairy
Associate

Hello! Im using STM32Cube IDE version 1.12.1.Im having isssue with including the header file "ai_platform.h " and "ai_datatypes_defines.h".I have installed X-cube-AI extensions  and all other required extension of Artificial Intelligence.I am getting the error message of "no such file or directory" .I request you to look into the issue.

Thank you !

3 REPLIES 3
AScha.3
Super User

look, are this "missing" files in path ? maybe, you have to add path... if not there.

AScha3_0-1688228961856.png

 

If you feel a post has answered your question, please click "Accept as Solution".

Where can I find these missing files ?Middlewares files are missing in project file.I downloaded the STM32 Cube IDE on 28th of June 2023. Is there any further update ?

 

no, you misunderstood.

if download was ok, all needed files should be there. 

just maybe , a path to use/include is wrong or missing; that i wanna show.

so first take an example project, to see, all is working.

and for missing .h -> search file on your disk, then control, that this is in path-settings (or add, if not there)

 

If you feel a post has answered your question, please click "Accept as Solution".