2025-02-12 9:41 PM
Hello!
I've been tasked to use the STEVAL-PROTEUS1 board with the ISM330DHCX to detect anomalous motor behavior. I've confirmed the board works fine when using other firmware and works as a WCID & MSC with datapro. However, when I try to flash the auto generated datalogger firmware from Nanoedge AI for serial data collection (via FUOTA), it does not create a COM port I can point the serial monitor at. I'd be grateful if someone could advise me of mistakes I might've made along the way, or if flashing via FUOTA does not work because there is a second flash bank or something similar. While I do currently have access to a STLINK V3-MINIE, I would prefer if flashing via FUOTA was an option, as it makes for an easier showcase.
Thanks in advance
Haze
Solved! Go to Solution.
2025-02-27 9:51 PM
Hi @Julian E.
A late update, but the board now successfully broadcasts itself when using the HSE BLE stack provided with PDMWBSOC2. The LSE stack didn't seem to work even after complete resets, but that's a now not an issue for me given the HSE stack works fine. As you hinted, using the PLL from the HSE seems to have fixed the RF mismatch that was caused by the LSE stack. Thanks for all the help.
Haze