2019-04-08 5:02 AM
Hello,
I want to sense period of 4 pulses using Analog Watchdog. I am using SPC560B40L3(100Pin controller). My requirement is to sense the Analog window voltage.
Ex. Square wave Pulse varies from 0.5V to 4.5V. And if I put my thresholds for every pulse on 1V(LOW threshold) & 4V(HIGH threshold). Is it possible to detect individual pulse transition period measurement?
Thanks,
Ashok
2019-04-11 1:34 AM
Hello ,
i think that it is possible
By using emios ,
Input Period Measurement (IPM) mode cf RM017
Best regards
Erwan
2019-04-12 9:22 AM
Thanks for response.
I think by using IPM I'll be able to measure total pulse not half pulse(High/Low Period) please correct me if I am wrong. By using Analog watch I want to measure half pulse period for multiple channels.