cancel
Showing results for 
Search instead for 
Did you mean: 

spc5.drive.cloudforge.com

Erwan YVIN
ST Employee
Posted on December 21, 2017 at 11:04

SPC5Studio 5.7.1 is available

Dear All ,

SPC5Studio 5.7.1 is available

*** Highlights ***

Here are the changes coming with SPC5Studio v5.7.1

For Selected Customers:

================

- Network bugs fixing

Use these following update sites :

http://spc5.drive.cloudforge.com/projects/spc5releases/SPC5Studio/updates5

http://spc5.drive.cloudforge.com/projects/spc5tools/updates

(New update Site for free GCC feature and PLS Feature)

http://hightec.spc5studio.com/

(Hightec compiler)

                  Merry Christmas

                                 Erwan

#spc58 #spc5studio #spc56 #spc57
This discussion has been locked for participation. If you have a question, please start a new topic in order to ask your question
11 REPLIES 11
Guglielmo Spina
Associate II
Posted on January 18, 2018 at 12:23

PinMap editor for SPC570S50 is available?

Posted on January 18, 2018 at 15:11

Yes , it is ;)

Guglielmo Spina
Associate II
Posted on February 01, 2018 at 15:54

it not working fine, because when I click on PinMap editor Link error message appears:

'Device specific model 'SPC570S50E1' not supported!'

Posted on February 02, 2018 at 10:25

Yes , it is supported

have you installed the last version of the pinmap  ?

Cf SPC5Studio marketplace

           Best regards

                     Erwan

Patriks
Senior
Posted on February 11, 2018 at 13:20

Does SPC5 Studio support new SPC58x microcontrollers? If not is it planned to implemented support for theses controllers soon? I´ve installed the new SPC5 Studio release and would like to experience with SPC582B-DIS board.

Erwan YVIN
ST Employee
Posted on February 12, 2018 at 09:42

Hello ,

Please refer to the installation procedure after downloading SPC5Studio

for SPC58x family ,it is for selected customers 

could you send an email to

mailto:credentials@spc5studio.com

 ?

if the marketing guys are ok , we will send you a login/pass for spc58x support

  Best regards

       

              Erwan

Posted on June 05, 2018 at 16:05

I have the latest version of pinmap installed from the marketplace but I still have the same problem. I'm using the SPC570S-DISP eval board.

Posted on June 06, 2018 at 09:52

Hello Yalin ,

Could you try to use the official update site ?

Use these following update sites (Mass Market) :

/external-link.jspa?url=http%3A%2F%2Fspc5.drive.cloudforge.com%2Fprojects%2Fspc5releases%2FSPC5Studio%2Fupdates5

/external-link.jspa?url=http%3A%2F%2Fspc5.drive.cloudforge.com%2Fprojects%2Fspc5tools%2Fupdates

(New update Site for free GCC feature and PLS Feature)

/external-link.jspa?url=http%3A%2F%2Fhightec.spc5studio.com%2F

(Hightec compiler)

/external-link.jspa?url=http%3A%2F%2Fflasher.spc5studio.com

(Flasher)

Anyway , update by proxy could generate some issues ?

Best regards

Erwan

Posted on June 06, 2018 at 09:59

Hi Erwan,

I am using the official update sites, as can be seen in the attachment.0690X0000060L8XQAU.png