cancel
Showing results for 
Search instead for 
Did you mean: 

it's my first Project with a SPC560D40 an SPC5 Studio. I'm trying to generate PWM-Signals on the Pins RA0 to RA5. When I look in the eMIOs Settings of the SPC560Dxx HAL Driver Component, I can only activate eMIOs group 0 (Channel 9..15) or Group1 (Channel

Rajesh  kumar
Associate
Posted on March 09, 2017 at 07:28

it's my first Project with a SPC560D40 an SPC5 Studio. I'm trying to generate PWM-Signals on the Pins RA0 to RA5. When I look in the eMIOs Settings of the SPC560Dxx HAL Driver Component, I can only activate eMIOs group 0 (Channel 9..15) or Group1 (Channels 17..23) but RA0 to RA5 should be Channel 0..5. For these Channels I can only activate ICU drivers. 

#pwm
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Erwan YVIN
ST Employee
Posted on June 14, 2017 at 10:46

Hello Rajesh ,

Sorry for the late answer.

Yes, we have implemented like this.

You can update the driver by using the Patch mode mecanism in patching the driver in lib/src lib/include folder.

Do not hesitate to contribute in

https://github.com/microwan/spc5-hal

 

             Best regards

                     Erwan