2017-06-06 2:51 AM
Dear All ,
SPC5Studio 5.3.2 is available
*** Highlights ***
Here are the changes coming with SPC5Studio v5.3.2
- Serial Read not fully working in Linflex_v1 driver
Here are the changes coming with SPC5Studio v5.3.1
- Update the max values of K2 clockpoints
- Update Velvety Header File
- SPC560p.h header file issue: MDIS bit missing in the definition of MCR register in PIT tag
- Write one to clear (w1c) register issue
- Pinmap for BGA: allow flip of image to see device in order to have A1 ball in top left corner
- Several bugs and improvements, please refer to
https://community.st.com/community/automotive-mcus-community/spc5-automotive-mcus/activity
(SPC5Studio part)*** Notes ***
- Make sure to read the SPC5Studio Users Guide and Components
Writers Guide in
the help section.
Enjoy SPC5Studio,
The SPC5Studio Team.