2014-05-09 5:46 AM
Appart from the fact that there are no specific examples for it, i have tried to do something with spc56ELxx OSLess CAN example from another board, and even though leds blink, there is no CAN data generated.
I would really appreciate if i could get this to work. And regarding FlexRay, are there any resources available for it? Thanks! #can-spc56el70l5-flexray2014-05-13 7:15 AM
Hi,
The existing CAN demos use an internal loopback mode, messages are exchanged internally so nothing is visible outside. If you need to adapt a demo to another board, proceed as follow: - Copy/paste the CAN project in the ''Project Explorer'' and give it a new name (optional). - Open configuration.xml.. - Select the ''drivers'' component, go in the CAN section and open the only configuration you see there, unselect the loopback mode. - Select the ''board'' component and load the preset for your board using the ''open'' icon in the configuration view, this will setup IOs for your board. You don't need other settings because the two boards have the same oscillatory frequency. - In the board component again you have to setup the CAN pins for CAN, see the Reference Manual and the board schematic. Giovanni2014-05-19 8:48 AM
2014-05-22 1:53 AM
Thank you very much, i will test it this afternoon and come back with results.
By the way, what about FlexRay? Regards, Javier2014-05-28 11:52 PM
Hi,
FlexRay support is not planned for SPC5Studio at this point. A FlexRay driver is available in the AUTOSAR MCAL package for SPC5 devices. Giovanni2017-06-01 2:28 AM
Hello,
were there any changes regarding FlexRay? Are there any examples for that?
David
2017-06-01 9:37 AM
Sorry David ,
At the current time, it is not planned for SPC5Studio release.
Best Regards
Erwan
2017-06-16 1:24 AM
Hello David ,
on Mass Market point of view (RLA & HAL), we have no FlexRay drivers
About AUTOSAR MCAL on SPC56 L, you can find some information on this following link.
Best regards
Erwan
2017-06-16 2:31 AM
Hello,
but as far as I understand it still is possible to make use of flexray right?
Giovanni mentioned the
AUTOSAR MCAL package for SPC5 devices, what is this exactly? Is this the drivers for FlexRay?
Is this something st offers or from a third party?
Thanks in advance,
David
2017-06-16 3:55 AM
Hello Erwan,
does this now mean that the SPC56 L can be used for FlexRay applications or not? Because the link you sent does not show any signs of FlexRay.
If it is still possible to use the FlexRay is there any possibility that I can get a sample program?
Best Regards,
David.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.