2020-11-03 5:00 AM
We are selecting a controller for our new Automotive project with CAN - FD connectivity,
We are now shortlisted SPC560D controller, But it is having FlexCAN.
So want to ask you that, Is CAN FD and FlexCAN is same?
2020-11-13 7:49 AM
Hello,
CAN-FD and FlexCAN are not the sane
FlexCAN support CAN protocol but does not support CAN-FD protocol.
If you are looking at automotive microcontrollers with CAN-FD please have a look at SP57/SPC58 family:
https://www.st.com/en/automotive-microcontrollers/spc5-32-bit-automotive-mcus.html
and then select SPC57 or SPC58 devices.
Or see this brochure (just for SPC58 Chorus devices):
Regards,
Giuseppe