2014-08-28 2:35 AM
Hi,
I am planning to use TDA7498MV for Active Speaker application. According to Datasheet Rev4, I am confusing about package. I need a EPU type package because of big out-put power. Description and Table-1 said EPU,however illustration and Fig-26 show EPD. Which is correct? Please confirm. Best Regard Hiroshi Furuno2014-08-28 2:54 AM
hi Hiroshi ,
in fact TDA7498MV is EPU type , the thermal pad is on the top of device , due to the dissipation power is much higher when the output power is reach 100W , so an external heat sink must be added to cool down the device and maintaion rated output power . thanksFrom: furuno.hiroshi
Posted: Thursday, August 28, 2014 11:35 AMSubject: TDA7498MV EPU Up or Down?Hi,
I am planning to use TDA7498MV for Active Speaker application. According to Datasheet Rev4, I am confusing about package. I need a EPU type package because of big out-put power. Description and Table-1 said EPU,however illustration and Fig-26 show EPD. Which is correct? Please confirm. Best Regard Hiroshi Furuno