2016-02-24 12:38 AM
Hi,
Could you please specify the exact pattern of behaving of TDA7496 at 12V input voltage. When we did a prototype the out put is getting clipped.Could you please specify the values to get 11V Output wave? #tda74962016-02-24 1:24 AM
Hi Meria ,
you can refer to output power vs supply curve , for 11V power supply input , the output power is around 1W 1% THD @ 4 ohm load , so the unclipping output level is around 2V RMS . for 8 ohm load , it will be around 0.7~0.8W , then the unclipping output level will be around 2.4V RMS . Thanks to choose ST device. YT