2013-11-11 4:50 AM
During the APWorkbench setup process FTDI drivers are optionally installed. Can you explain what it is for and if I should install it?
2013-11-12 6:13 AM
FTDI drivers are used by APWorkbench suite to communicate with the hardware
http://www.st.com/web/en/catalog/tools/FM116/SC1028/PF253187
, via USB. Driver installation is required in case evaluation boards using APWLink have to be operated (typically allhttp://www.st.com/soundterminal
amplifier boards). FTDI drivers are not required for MEMS Microphone evaluation kit since it makes use of a different USB interface,http://www.st.com/web/en/catalog/tools/FM116/SC1028/PF258331
. Updated drivers can be downloaded from FTDI website (D2XX version): Note: admin rights are required to install FTDI drivers.