2014-02-04 7:59 AM
Could your recommend a class D amplifer,the supply voltage is 12Vdc,mono BTL,output 50W~100W.Thanks!
2014-02-09 6:29 PM
hi naue_b ,since the output power had been limited by supply votlage , even the load impedance is 2 ohm , the max 10% THD output power is around 35W, it's far away from your target output power . but if the supply votlage was 20V, TDA7498E can meet your reqirement.
Thanks