Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Most recent activity
In the documentation for STM32WB09 it is written that the output impedance of the chip is 40 ohms. It is also written in the document AN5526 on page 5. And in the documentation for MLPF-NRG-01D3 chip it is written: Transmission line between STM32 and MLPF is dimensioned to 57 ohms characteristic impedance.What should be the impedance of the transmission line between STM32 and MLPF?And another question, in the same AN5526 document it says that the thickness of the double layer PCB should be 0.5mm.At the same time there is a two-layer board STEVAL-IDB012V1. Does it really have a board thickness of 0.5mm? If the thickness is 1.5mm, can 1.5mm boards be used with the STM32WB09 chip?
HiI am trying to interface the STM32WLE55x lora module to a pulse counter. when I tried with interrupt as a counter (as i have to count the pulses!!!) its taking 123mA current at the time of sending the data to server and on ideal condition it is taking around 5 to 6ma!!!! This seems very high for me. I am trying to develop this on a battery so it will kill my battery. I have tried using LPTIM with LORA wan but its not taking as interrupt for LPTIM even the LORA is getting connected or unconnected, the interrupt is not performing tasks what it suppose to. any one have idea to reduce current in interrupt mode or how to enable LPTIM interrupt so it can perform the tasks. Thanks
I'm working on a project with the STM32WL55JC microcontroller. Before testing the LoRaWAN_FUOTA_DualCore application, my LoRaWAN setup was functioning correctly with all example applications.However, after flashing the LoRaWAN_FUOTA_DualCore application, I noticed that only this application is working. While other applications like LoRaWAN_FUOTA, LoRaWAN_End_Node, and LoRaWAN_End_Node_DualCore are functional in terms of peripherals, my device is unable to connect to the LoRa gateway.Could you help me understand why it’s only working with the LoRaWAN_FUOTA_DualCore application?
I 've made a realy simple app for testI'm using only 1 i2c and 1 spi and 1 gpio as input and 2 as outputI've set all unused gpio to analog to lower currentafter init it starts advertising and goes in STOP2 mode for 10 secI can see after the boot around 10µA of minimal current with spikes every 800ms witch is my advertising periodafter 10sec RTC wakes up CM4 it cancel advertising and goes OFFbut when it goes off it draws around 1mA and some time with litles spikesto solve I've try several things when entering OFF mode in PWR_EnterOffMode :- I've cut all clocks for spi/i2c/ipcc and and shut down C2 (CM0)HAL_IPCC_DeInit(&hipcc);HAL_I2C_DeInit(&hi2c1);HAL_SPI_DeInit(&hspi1);LL_AHB1_GRP1_DisableClock(LL_AHB1_GRP1_PERIPH_CRC);LL_PWR_DisableBootC2();- I've set all gpio to pull-down to avoid artifact on other of board's IC- set all gpio as output and lock them using LL_PWR_EnableGPIOPullDown() to avoid relaxing gpio when going offbut I have no results and lacking of ideaIf anyone h
I've looked through many examples (in particular p2p client ) but I can't find any that sends payload that's made of array ```uint8_t pPayload[] = {0xFF, 0x01, 0x00, 0x05, 0xAA};uint8_t payloadLength = sizeof(pPayload);ret = aci_gatt_write_without_resp(aP2PClientContext[index].connHandle, aP2PClientContext[index].P2PWriteToServerCharHdle, payloadLength,&nbs
Hello,I have developed a custom board around the WB5M and I am working on adding OTA support to it using the sample code from CubeWB -> Projects -> NUCLEO-WV15CC -> Applications -> BLE -> BLE_Ota.I have modified this code to use CMake (following the pattern of my app firmware which is customized from a template CubeMX / CMake application) and then made the changes to the sample app to use stm32wbxx_hal_driver and CMSIS_device_wb with STM32WB5Mxx defined. I have turned off CFG_LED_SUPPORTED and CFG_BUTTON_SUPPORTED since there is no BSP associated with my custom board.So far the code compiles, flashes, and seems to be trivially working -- e.g. I can use a BLE app to see advertisements for BLECore with Local Name STM_OTA with the manufacturing data in the advertisement. I can connect/disconnect to the device, though no services are advertised (I believe this is 'normal' OTA behavior?). I have not yet connected an OTA app to attempt a firmware fla
Good day, We have a battery-operated device using the STM32WL55.The battery voltage is regulated to 3.6V as supply to the STM32.We have found when the battery runs flat, the STM32WL5 would often need to be reprogrammed. This doesn't happen when we plug the battery out. The below is the 3v6 power rail when I turn the input down to 1.4V. Our MCU brown-out is set to default. Any suggestions of what might be happenign or what we need to look at?RegardsDouglas
Yesterday evening I worked on an application for a Nucleo-WL55JC and STM32CubeIDE could connect to the ST-LINK just fine. I closed my PC and this morning started it again. I am trying to upload code to the CM0Plus core and now I am getting the following error: Target unknown error 32Error in initializing ST-LINK device.Reason: Unknown. Please check power and cabling to target. Things I did to diagnose and solve:I have checked the USB cable which is perfectly fineI changed for another USB cable which did not change the situation.I used a similar Nucleo board which was never used and got the same error.I checked the settings in the debug configuration. All seems fine.I tried to access and erase the chip with STM32CubeProgrammer -> THIS WORKS FINEI made a new project and tried connecting to the chip with STM32CubeIDE. This does not work.I tried to upload code to the CM4 core and this worked. Does anyone know how to solve this? I am on a very tight deadline an
Hello all,I want to use the STM32WB5MMG module for a project which requires an RTC.The datasheet states the module integrates a 32.774 kHz LSE crystal. That seems a bit strange to me because the standard clock for LSE is normally 32.768 kHz. Checking the reference manual RM0434 there does not seem to be any reference to using a 32.774 kHz clock.I would like the RTC time to be as accurate as possible, is 32.774 kHz ok to use for the RTC? I guess I would need to somehow offset the faster clock to keep correct time.Here are some calculations I did, which I have no idea if they are correct.It seems that a 32.774 kHz clock divided by 2^15 = 1.000183105.That equals 0.001000183 ms offset from the ideal 1 second per clock period.Multiply by the number of seconds in a day, 0.001000183×86400 seconds = 86ms offset per day.If you have any thoughts on the matter, let me know!Thanks!-Eric
Dear ST Support Team,I am working on a project using the STM32WB5MM module, where I am trying to create a custom BLE service under Server mode, and also enable FreeRTOS for task management. However, I’ve encountered an issue where the Custom Server option in STM32CubeMX disappears when I activate FreeRTOS.Here’s a summary of my setup:Microcontroller: STM32WB5MMSTM32CubeIDE Version: 1.16.0BLE Middleware: STM32_WPAN (BLE stack enabled)RTOS: FreeRTOS (latest available in STM32CubeMX)When FreeRTOS is not enabled, the Custom Server option appears normally, allowing me to configure a custom BLE service. However, as soon as I activate FreeRTOS, the option disappears from the BLE Server mode configurations. I have ensured that the BLE stack is configured properly and that I am using the peripheral role for BLE.I have also checked memory allocation and attempted to adjust heap sizes, but the problem persists. Could you please advise on why this conflict occurs and how I can enable both Fr
Hi there.I'm trying to use the STM32WB0 (NUCLEO-WB09KE) in HCI Controller mode with our Bluetooth Stack: https://github.com/bluekitchen/btstack/I found the BLE_Transparent application in the STM32WB0 Firmware package which provides HCI over the virtual Serial Port of the ST-Link.This works until a connection is established. Then, the ST BLE Stack initiates an ATT MTU Request and informs us via a custom HCI Extended Event.How can I disable the included BLE stack in the BLE_Transparent example and use the STM32WB0 with an external Host Stack?Thanks, Matthias Ringwald, BlueKitchen GmbH
I've found something curious in the code generated by CubeMX for a BLE application on STM32WB. In APP_BLE_Init we have this:/** * Do not allow standby in the application */ UTIL_LPM_SetOffMode(1 << CFG_LPM_APP_BLE, UTIL_LPM_DISABLE);My understanding is that this prevents CPU1 from going into standby while CPU2 is booting. Then, in APPE_SysUserEvtRx, we have this:UTIL_LPM_SetOffMode(1U << CFG_LPM_APP, UTIL_LPM_ENABLE);Again, my understanding is that this is in response to a message from CPU2 indicating that it has finished booting, so standby mode can once again be enabled.However, what I've just noticed is that these two calls use different IDs (the first disables standby mode for CFG_LPM_APP_BLE, and the second enables it for CFG_LPM_APP). The effect is that standby mode is never re-enabled when CPU2 finishes booting.These are the only two calls to UTIL_LPM_SetOffMode in the generated code, so it seems unlikely that the change in ID is intentional--why would we see exact
How to erase STM32WLE5JC so that I can put my binary in the Seeed Studio Wio-E5 module. Web says changing the lock bit from hex value of ??? to ???. Where can I set it? TIA
Hello STM32 community, I'm currently working on implementing Zigbee applications on my STM32WB55 Evalution boards, and I'm looking to create custom clusters. I've gone through the documentation custom-clusters, but I'm a bit confused about the procedure. Could someone please guide me on how to create custom Zigbee clusters on STM32? Is there any GUI cluster configurator tool available in STM32CubeIDE?Any step-by-step instructions or examples would be greatly appreciated.Thanks in advance!Best regards,Naani Ch
Hi,I'm working on implementing attribute reporting on the Zigbee STM32WB55 Evaluation boards. I've attempted to configure attribute reporting in the Zigbee_DevTemp_Server_Coord and Zigbee_DevTemp_Client_Router baseline examples. However, I encountered an issue on the server side where I am unable to perform the Write operation on the attributes. ([DEV TEMP]Failed to initialize initial Temperature) During my investigation, I came across two APIs, namely ZbZclAttrReportKick() and ZbZclClusterReportCallbackAttach().Interestingly, without using ZbZclAttrReportKick(), the report callback implemented on the router side is not being triggered. I'm curious about this behavior. The comments suggest that the application might disable automatic periodic reporting, but I'm unsure why this is happening.Is it not possible to receive the callback output on the client side without calling ZbZclAttrReportKick()? Here are the comments on ZbZclAttrReportKick(); /** * This
I've been having a lot of trouble getting all of the online BLE examples to work and was hoping someone could steer me in the right direction. In every example they state that the RFWKP Clock Mux should be set to LSE but whenever I do that the main loops runs once then hangs somewhere in MX_APPE_Process() but I'm not sure where. Interestingly if I setup a timer and ADC (to give it something else to do) that part works just fine - my ADC loop just reads a few values every second then toggles and LED. If I set the RFWKP Clock to HSE then it seems to work fine. I thought it was a problem with my custom board but this happens with the P-NUCLEO-WB55 board as well.I'm using STM32CubeIDE version 1.14.1 and have the latest version of the FUS and wireless stack installed.
Hi , I see in the Datasheet in Table 31 some reciever parameters .I need to know what is the Dynamic Range of the Reciever in the STM32WLE5 . can you point me to which parameters should I look at ? Thank youViola
hi, I have two B-WB1M-WPAN1 cards and I would like to create a program that works as a client server, so one card will act as a server and then other client cards will send messages to it via BLE, I saw the example proposed by the company "BLE_HR_p2p_Sensor" which might look like what I want to do but I haven't quite figured out how it all works.Where can I find, for example, a complete file with commands useful for BLE transmission?Then if you have any advice they are welcome, I would also be curious to understand how the connection through the application from the phone to the card works.
Hello, I have a question regarding having both library (from the example files) SubGHz and LoRaWAN on the same microcontroller STM32WL5MOC at the same time and my idea is to use a switch to choose which on i would like to use depending in the case of use.
Hello,This message is for ST team.I attended the webinar on STM32WB0 MCUs, but I didn't receive the e-mail that was supposed to follow, including the links, recording and voucher for the demonstration board.What happens ?PS: I'm posting here because I'm having trouble connecting to online support.
Hi , in the Datasheet there are few interfaces which are marked as "alternate functions" for DEBUG_RF or DEBUG_SUBGHZSPI. ( Table 20 in the Datasheet)But , I didnt find any info regarding what can I use those function for ? for example - Can i access this SPI from external pins ? is there additional Info regarding those debug capabilities and what each signal is used for ? ThanksViola
Hello, I have configured a Zigbee network using an STM32WB55 MCU with 1 coordinator device and 5 end devices. However, since I cannot check whether the Zigbee connection is lost or not, I am resetting the end devices every 1 minute using NVIC_SystemReset();. Instead of this, I am looking for a function that checks the connection status. Is this possible? During debugging, I see that the static void APP_ZIGBEE_NwkForm(void) function is used for joining the network, but after joining the network, there is no check for whether the device is still connected. I would like to check if the device is still connected to the network after some time and if not, call the function to rejoin the network. Is there a variable or function available for this check? I would greatly appreciate your support.
Hi,I have used a custom board with an STM32WB55CG MCU to successfully connect to a Tuya Gateway and also a Homassistent/Zigbee2mqtt setup with the OnOff functionality.As next topic I wanted to add a color control functionility and tried several optins (Profile ID HA or ZLL) and several functions of the color control cluster (such as step_color_xy or move_to_color_xy).In my Homassistent, the board was successfully detected (already one step ahead of my trial with Tuya) and the clusters were detected correctly. However, sending any color request from the UI in Homassistent did not work and no command was received on my board (reading the Debug messages with UART), while the OnOff functionality was still there.Since the UI gives also the option, to send commands directly, I tried to send a command to my endpoint, with the cluster 0x0300 (Color Control) and 0x07/0x09 (move_to/step_color_xy) and an arbitrary payload (Zigbee2mqtt makes sure that the format is correct). Neither of t
Hi, I am currently working with the STM32WB5MMG MCU and looking for some insights regarding its power consumption. Specifically, I would like to know:What is the current consumption when the MCU is in STOP2 mode with the RTC enabled?If anyone has experience or data on this, please share your insights. Any references to documentation or practical measurements would be greatly appreciated.Thanks in advance!
Hi all,I check with STM32WBA55 datasheet have description can supported external PA. But FW SDK(STM32Cube_FW_WBA_V1.4.0) released notes exist below description. It look Known Limitations is not support EPA, usually need logic control between FEM and radio.Can you let's know, Which FEM PN be recommend and will be supported in SDK?Best Regards,Ethan Chen
WATCH ON-DEMAND | STM32 Summit 2026
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.