Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Most recent activity
I have identified from this post and AN5270 that ACI_GAP_TERMINATE and HCI_DISCONNECT may be viable functions to call from a peripheral device to terminate a BLE connection. My employment of these functions causes no change, similarly use of ACI_GAP_SET_NON_DISCOVERABLE has no effect on whether or not my peripheral (STM32WB) continues advertising. Furthermore I'm unsure of how to extract the connection handle that I need to pass to ACI_GAP_TERMINATE or HCI_DISCONNECT as a parameter and have assumed its value to be 0 as I have only one connection. I have tried overriding HCI_LE_CONNECTION_COMPLETE_EVENT to extract the connection handle however it doesn't seem to get called at all, even when a successful connection between STM32WB and Phone Application are made.
Hi. I have problem with connect to NUCLEO-WL55JC nucleo via ST-Link Utility. I am unable to connect with any option (hot plug, connect under reset etc.) or hardware reset to STM32WL55 MCU on board (there is some demo soft which is unable to erase). Same thing on both boards. Anyone have similar problems? Thanks for any answers.
STM32WB5MM-DK Board User Manual is not available in the product page to download. Can I have a copy of the User Manual please?
Programming manual PM0271, page 4, current features supported on Bluetooth specification v4.1, it is said that it only supports being slave of up to two masters simultaneously.But as for the standard, the maximum connections number would be 8. I'm trying to use "server" and "client" examples, using full stack, but the server can only connect to 2 clients. After this, it can't put server on advertising mode (I'm starting again the advertiser after every connection). Currently I'm using STM32WB v1.11.1 package. I've tried v1.9.0 and v1.10.0 with the same limitation.Is there a way to connect a slave to more masters?
Erik Cool+32 2 206 9367Tervuursesteenweg 303 | B‑1820 Steenokkerzeel T. +32 2 206 21 11 | www.skeyes.be
In STM32WLE5JC MCU, the SPI data length is set to 8 bits, and the corresponding receiving FIFO is also set to 8 bits, but the final receiving and sending data is 16 bits.1. SPI-CR2 registers during transmission are as follows:It can be seen from the figure that CR2 is 0x1708, the threshold of FIFO is set to 8 bits, but the data length of DR is 16 bits: 0x01302. the CR2 register in 2.STM32WL is described as follows:
I built the project with CubeMX 6.2.1. I have added the call in main to the sequencer. I have added the sequencer header file. I have added the IPCC IRQHandler functions to stm32wbxx_it.c.The project builds fine and downloads to the NUCLE0 WB55. It starts up and advertises as expected but it will not let me connect to it.Attached is my CubeMX project.Any help will be greatly appreciated.
..
I wan't to power both cores with 1.8V and, only when using the radio, use 3.3V.I have seen there is a VDDRF pin to power the radio but data sheet says it must be connected to the same supply as VDDMiguel
HelloI try to create a BLE App with CubeIDE, running on P-Nucleo-WB55 board.I have updated firmwares on my board (FUS, BLE Stack, STLink).The code is generated on CubeMX and imported in CubeIDE.Like many users, I have corrected Heap_Size and Stack_Size values to resolve HardFault issues found in this forum. All seems to be ok… But my board doesn’t advertise.After debugging, I discover that program never goes in APPE_SysUserEvtRx function (in app_entry.c), and so the APP_BLE_Init is never called… Initialization in appe_Tl_Init seems to be good. I have compared BLE_p2pServer.ioc configuration and mine, no significant difference.I think I have made a mistake but I don’t find where. Any idea?
BLE5.0 has the Periodec Advertising feature.How can I use Periodec Advertising?And, is there a sample program for Periodec Advertising?
Does STM32WB supports AOA (angle of arrival) and AOD (angle of departure)?
Hi.I want to write desktop application using STM32CubeProgrammer API to load FUS and stack to STM32WB. But in documentation I can`t find any mentioning about how to start FUS, update FUS and load stack.Or does the API do not give this opportunity?
Hi all. I found out there are specific DEBUG_SUBGHZSPI_* alternate functions (DS13105 STM32WLE5xx). But there is not much information about these functions. Can these AF be used to 'mirror' SUBGHZSPI pins for debugging / captures ? Thanks Olivier
Hello all,I was developing LoRaWAN applications on MICROCHIP products for many years, recently I switched to STM32 platform. I have developed many applications with STM32L0 + SX1272 combination which worked perfectly. Now I have decided to move to new STM32WL series. I am running my applications on Nucleo board very well but when i switch to my custom board i have some suffer because of TCXO. Since I needed PB0 pin for other purposes I decided to use external HSE oscillator instead of TCXO. Now I try to run my application on my custom board but it seems not working. How can I run LoRaWAN_End_Node application from STM32Cube_FW_WL_V1.0.0 without TCXO? Here you can find the reference nucleo design from ST and my oscillatos at above images. Thanks for help.
I have used the Device Configuration Tool to set up an SPI1 peripheral on PB3, PB4, PB5 with manual control of the chip select, and polled (not interrupt driven). Writes to SPI slave chips registers execute without error, but register reads give a HAL_TIMEOUT error in HAL_SPI_TransmitReceive() because the RXNE flag (data in fifo) is never set.The clock is enabled to the SPI and I can read/write SPI registers. CR1, CR2, SR values look sensible. I have not yet tried different pins, or SPI2.Has this been tried, and can someone point to a known working example?Unfortunately, the SPI examples that ST provide don't build (at least for me, with Eclipse), but in any event they are special cases: two processor chips connected, one as master and one as slave, with no chip select. A real example (e.g. talkig to an accelerometer chip) is missing.
Hi everybody, yesterday I was working with my Nucleo68 board of the P-NUCLEO-WB55 pack as always, however something go wrong after to did this:I modified the WWDGSW and IWDGSW option bytes with STM32CubeProgrammer (from checked to unchecked, and apply), option bytes were programmed successfully, run my application and all ok.After return the WWDGSW and IWDGSW option bytes with STM32CubeProgrammer (from unchecked to checked, and apply) the options bytes doesn't programmed and message apears "Error: Option Byte Programming failed", I tried some times more and nothing.I desconnected and connected again the Nucleo68 USB cable but when I read its data a message apears with "Error: Data read failed". I can't read any page of the flash:I guess that I can erase flash because apears the following message when I erase a sector:But when I download a file this failed:Checking the RM0434 Reference manual the option bytes are ok because are in ST production value, here the option bytes of my STM32WB
I am using the STM32WB55 ADC with the internal reference VREFBUF set to 2V5. To save power consumption, the application disables VREFBUF before going to sleep and enables it just after waking up. The problem is that I am making measurements with the ADC just after wake-up and I am getting results slightly lower than the real values.When I enable VREFBUF I do the active wait for the VRR flag and I see that it takes about 50us to settle. On the VREF+ pin I have a 100nF capacitor. If I do a delay of 500us then, the measurements with the ADC are correct.What could cause this difference in the measurements? Why is the stabilisation time of VREFBUF so low?
If I use STM32WL as RF tranciver and using the (G)FSK modultion or other modulation with multiple users, Will STM32WL asigne a carrier frequency automatically for each user to achieve the FDMA as PMR/DMR system in walkie talkie?
Hi, I am running the BLE_DataThroughput example for the STM32WB55 with two boards as described in the documentation- one set as a client, one as a server. I have connected the client board to a desktop PC via UART, and I am monitoring the output with PuTTy. With this setup, the highest data throughput rate I get is ~ 98 600 bytes/s as reported at the UART by the board. This is with PHY = 2M. When I press the SW2 button on the baord it switches to PHY = 1M, and the data throughput rate falls to ~2 500 bytes/s. My question is whether this is normal and how can I get the advertised 2 Mbit/s datarates for this chip, or at least something closer? The current data rate corresponds to ~ 0.8 Mbit/s. I referred to AN5289 Building wireless applications withSTM32WB Series microcontrollers, section 7.6.5- How to maximize data throughput where it is advised that I set the connection interval and connection event length at 50 ms, which I did correctly as far as I can tell. The effect this
Hi there, I'd like to know if the USB port on the stm32wl55 can be used as a virtual com port and if so, how to achieve that.
Hello,I use a STM32WB55RGV7 microcontroller. Doing the hardware layout I'm confused about the antenna filter: - I can't get the band pass filter LFB182G45CGFD436 in small quantities, which is used in the P-Nucleo-WB55 - the low pass filter LFL212G45TC1A007, wich is used in AN5165, is end of life in about one year - AN5165 uses also another low pass filter MLPF-WB55-01E3, which makes a part of the other componets unnessesaryCould you give me a suggestion which of these filters I can use in my design reasonably future-proof?Thanks in advance.Holger
I have a custom hardware with an STM32WLE5C8Ux and I want to add functionality to it step by step. I'm using CubeMx to generate a project with success ,toggeling a GPIO works. I have not initalized external TCXO or LSE, they are populated but I want to first run a very simple program without LoRa or anything. I want to add FreeRTOS in the long run so I wanted to add an alternate Sys timer, I selected TIM17 as a Timebase Source.Then I generate the project and debug over the ST-Link V3 an, adapter and a J-Link 10 Pin debug probe. I power the hardware externally. I'm running the internal clock at 48Mhz. When I step through the debugger I stop at Function "HAL_NVIC_EnableIRQ(TIM17_IRQn);" inside of "stm32wlxx_hal_tim.c" Here is the output of my debugging Temporary breakpoint 4, main () at ../Core/Src/main.c:72 72 HAL_Init(); Breakpoint 3, HAL_Init () at ../Drivers/STM32WLxx_HAL_Driver/Src/stm32wlxx_hal.c:178 178 if (HAL_InitTick(TICK_INT_PRIORITY) != HAL_OK) Program stopped
Hi!I can't find the WLCSP59-Package at distributors like digi-key, mouser etc. It doesn't seem to be available. Does anyone know why?Is this a matter of time (not in mass production yet) or a matter of volume (only sold to specific customers)?If the former, when will it be available?If the latter, which conditions apply? (NDA, minimal quantity, etc.)regards,aaron
WATCH ON-DEMAND | STM32 Summit 2026
Already have an account? Login
Enter your E-mail address. We'll send you an e-mail with instructions to reset your password.